Technical FAQs

Ask a Question

What is the maximum number of Equipment node for the Magelis XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU Series?

Issue:
What is the maximum number of Equipment node for the Magelis XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU Series?

Product Line:
Vijeo Designer

Environment:


Cause:


Resolution:
The Magelis XBTGC / XBTGT / XBTGH / HMIGTO / HMISTO / HMISTU Series support up to 48 (limit) of Equipment nodes.
Was this helpful?
What can we do to improve the information ?