Technical FAQs

Ask a Question

Can the LCD front panel on the Quantum PLCs be disabled?

The only way to disable the front panel operations on the Quantums is to turn on memory protect.

You can, however, turn off the backlight through the LCD settings on the front panel.
Was this helpful?
What can we do to improve the information ?