Browse FAQs

How to hide RMS and Legends in Waveform in PME 7.2.2 web application?

Published date: 24 September 2019

Issue
Hiding RMS and Legends in Waveforms in PME 7.2.2 web applicaitons

Product Line
EcoStruxure PME 7.2.2

Environment
PME 7.2.2 Web Applications waveforms

Resolution

Replace the chart.js file PME installation folder\system\WebReach\Scripts with the file attached.
By doing this, two toggle buttons for Legends and RMS will be enabled on the left top of Waveform in Web application, users can use the buttons to switch on/off legends and RMS

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.