Technical FAQs

Ask a Question

Can the M340 CANopen interface be disabled?

Title
M340 CANopen Interface
 
Issue
M340 CANopen Interface
 
Product Line
M340 BMXP342010.2 and BMXP342030.2
 
Environment
unity Pro
 
Cause
N/A
 
Resolution
 No, The CANopen interface on the M340 CPU version BMXP342010.2 and BMXP342030.2 can not be disabled.
Was this helpful?
What can we do to improve the information ?