Technical FAQs

Ask a Question

Is it possible to force a discrete input while using Concept?

Yes. Follow these steps.
1: Open an RDE template (Online/Equal/Animated).
2: Enter the address of the discrete input in the address field.
3: Click on the Disable box
4: Enter a value of 1 or 0 in the the value field to force the input on or off.



 


Legacy KB System (APS) Data: RESL201503 V1.0, Originally authored by RoAl on 03/02/2010, Last Edited by RoAl on 03/02/2010
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?