Technical FAQs

Ask a Question

Can I add an expansion rack to an existing Quantum RIO drop using the CCOTF option?

No. It is not possible to add an XBE interface and backplane to an existing Quantum RIO drop using CCOTF.


Legacy KB System (APS) Data: RESL209870 V1.0, Originally authored by DaSo on 12/04/2012, Last Edited by DaSo on 12/04/2012
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?