Technical FAQs

Ask a Question

How do I setup the M340 BMXNOE01x0 Address Server for a TeSysT ?

M340 BMXNOE01x0  Address Server for a TeSysT
Setting up M340 BMXNOE01x0  Address Server for a TeSysT
Product Line
M340 BMXNOE01x0
Unity Pro
 The setting up of the BMXNOE0100 Address Server for DHCP/FDR is done by adding the TesysT device name (using TeSysTxxx, where xxx is the concatenation of the tens and ones rotary switches) into the Address Server page of the NOE along with the desired ip settings for the TeSysT.

As far as storing the required TesysT configuration file, The user must initiate the backup of the TesysT configuration file  by using the TesysT configuration tool to backup the LTMR controller’s operating parameters, by uploading a copy of the device’s parameter file to the Address server (BMXNOE0100) from the TesysT controller.

Note- Any time the LTM R controller configuration changes, the user should manually backup the new configuration file to the DHCP server (BMXNOE0100) with the TesysT Configuration tool by clicking Device → File transfert → backup command
Was this helpful?
What can we do to improve the information ?