Technical FAQs

Ask a Question

What causes Concept error "2219 - UD get values not finished, stop read is not possible"?

Issue:
  Error occurs when project is online and running.

Cause:

  One or more large animation services are active while the user attempts to stop one animation or the error can occur
because the previous transmission of values is not completely finished.
Closing animation tables quickly one after another or shutting down Concept with an animation running can also cause this error

Resolution:
 It may be necessary to recover by disconnecting & connecting again
Was this helpful?
What can we do to improve the information ?