Technical FAQs

Ask a Question

Can I download a project to the Unity Quantum PLC using the Unity Loader?

Issue:
   Downloading a project to the Unity Quantum with the Unity Loader.

Resolution:
   Unity Loader v8.0 added the ability to download a project to a Quantum PLC.  The Quantum PLC is accessible
over the Modbus port.
Was this helpful?
What can we do to improve the information ?