Technical FAQs

Ask a Question

What is the battery part number for the Momentum.

Issue:
What is the battery part number for the Momentum PLC adapters.

Resolution:
There is two different versions of the Momentum option adapters.
If the adapter has two batteries they are standard Alkaline AAA.
If the adpater has a single battery it is lithium. The part number to order is 170XTS15000.
 
Was this helpful?
What can we do to improve the information ?