Technical FAQs

Ask a Question

What is the causes of SAFF without safety configured in ATV32?

For example we know 3 possible causes of SAFF without safety configured in an
ATV32. They are as follows:

- Instability detected (around 10,5V) on the STO input.
- Pulse (like relay rebound) on the STO input
- Interruption of the internal communication
Was this helpful?
What can we do to improve the information ?