Browse FAQs

Can the Apogee card(VW3A3314) be used on the ATV71

Published date: 13 March 2019

Issue:
Can the Apogee (P1 or FLN) card be used on the ATV71

Product Line:
ATV71

Environment:
All

Cause:
Get an error when connecting the Apogee card to an ATV71.

Resolution:
The Apogee card can only be used on the ATV61 drive.
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.