Technical FAQs

Ask a Question

Is it possible to unforce a coil on the Quantum 140CPU6xx xx CPU without having Unity software?

Yes, a Cold Start will remove a force condition. On the double wide Quantum CPU's a "Reset" pushbutton located behind the LED window will initiate a Cold Start.
Simply power cycling the CPU would not remove the force condition. Power cycling is considered a Warm Restart.





R-71317


 
Was this helpful?
What can we do to improve the information ?