Browse FAQs

Is it possible to print is SoMachine Basic? Now known as EcoStruxure Machine Expert Basic.

Published date: 16 April 2019

Yes. As of April 1st a new install for SoMachine Basic came out that allows printing it is version 1.3 SP1 build 44532.
The current version as of 4/16/2019 is now called EcoStruxure Machine Expert Basic (formally known as So Machine Basic). and this also supports printing.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.