Technical FAQs

Ask a Question

PM8000 series front display simulator

Issue
Functionality of the PM8000 series meter may need to be implemented when instructing a customer through a setup procedure using a PM8000 series meter.

Product Line
PM8xxx

Environment
PM8xxx front display

Cause
Physical meter might be unavailable

Resolution
Please find in the attached .zip file OfflineMeter executables for the PM8000. Offline Meters, or meter simulators, are used on your Windows PC to emulate the meter hardware platform for the development and testing of meter application logic (a.k.a ION frameworks) using either ION Setup software or ION Enterprise Designer. Once the meter simulator is running, it can be accessed at the domain name "localhost" (127.0.0.1) with software on the same computer.
PM8000 display simulator
 
Was this helpful?
What can we do to improve the information ?