Browse FAQs

How can I monitor a communication break with the PLC using OFS V3.61?

Published date: 05 November 2018

You can monitor the #PLCQualStatus variable.  When OFS is communication to the PLC without issues the value is 192.  If the value is different than 192 it suggest a communication error to the PLC.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.