Technical FAQs

Ask a Question

What causes "runtime error code 52 bad file name or number" when launching Unity Pro?

Issue:
  Error message is displayed launching Unity Pro.

Product Line:
  Unity Pro programming software

Resolution:
  This error is usually caused by the user not being logged into the PC as an administrator with 'full control' rights.
Was this helpful?
What can we do to improve the information ?