Browse FAQs

What causes Unity build error: Parameter <length of module parameter word> out of range [value (7) not in [0 to 0]?

Published date: 28 December 2018

Cause:
    An error occured importing the project from Concept or Proworx.

Resolution:
    Delete the NOE in the Local IO bus and delete the Ethernet network and re-enter both.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.