Technical FAQs

Ask a Question

Is it possible to change the 140CRA31200, BMXCRA312x0 and 140CRP31200 from operating on VLAN1?

Title
140CRA31200. BMXCRA312x0 and 140CRP31200 on VLAN1
 
Issue
140CRA31200, BMXCRA312x0 and 140CRP31200 are hardcoded to operate on VLAN1
 
Product Line
Quantum , M340 PLC.
 
Environment
Unity
 
Cause
N/A.
 
Resolution
The 140CRA31200. BMXCRA312x0 and 140CRP31200 are indeed hardcoded to operate on VLAN1 and this cannot be changed.
 
Was this helpful?
What can we do to improve the information ?