Technical FAQs

Ask a Question

Can I use a BRS 3 phase stepping motor that has an "H" rated winding with Lexium SD32x type drives?

No, the BRS 3 phase stepping motors with "H" rated winding are for use with drives that operate at a maximum of 48 volts.
The Lexium SD32x drives operate with a 325 volt internal DC bus and therefore should not be used with "H" rated windings.  
Motor winding failure would result.

H rated windings are for use with Lexium SD315 type drives
Was this helpful?
What can we do to improve the information ?