Browse FAQs

How can I force the ATV-IMC to update the PIx / POx scanner?

Published date: 05 November 2018

When you start up the drive with an RUN Command the PIx /POx scanner is not updated.

You can add the following code in a POU to configure the scanner :

configureScanner : BOOL;

Code:

IF configureScanner THEN
         (* Initializing Cyclic data exchange Read*)
        DriveParameterCyclicReadSet(
                addrDRIVE_PI1:= 12741,     
                addrDRIVE_PI2:= 12742,    
                addrDRIVE_PI3:= 12743,     
                addrDRIVE_PI4:= 12744,  
                addrDRIVE_PI5:= 12745,     
                addrDRIVE_PI6:= 12746,     
                addrDRIVE_PI7:= 12747,    
                addrDRIVE_PI8:= 12748,     
            bExecute:= TRUE);

        IF DriveParameterCyclicReadSet.bDone THEN
            configureScanner := FALSE;
        END_IF
END_IF;

As soon as "configureScanner " is TRUE, the scanner configuration will be executed.
This should be done when drive status is different from "RUN".

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.