Technical FAQs

Ask a Question

Does the M580 platform support the use of Ethernet Global Data ?

Title
Does the M580 platform support the use of Ethernet Global Data ?
 
Issue
M580 platform does support the use of Ethernet Global Data
 
Product Line
M580 PAC

Environment
Unity 12 or higher

Cause

Resolution
Yes, the M580 platform does support the use of Ethernet Global Data through the use of the BMXNGD0100 module which is dedicated to global data.

Was this helpful?
What can we do to improve the information ?