Browse FAQs

What is the default TCP port assigned to the ModbusTCP protocol?

Published date: 29 November 2018

Title
ModbusTCP protocol TCP Port assignment
 
Issue
The Default TCP port number assigned to the ModbusTCP protocol
 
Product Line
Quantum, M580, M340
 
Resolution
 The default TCP port assigned for ModbusTCP is TCP port 502.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.