Technical FAQs

Ask a Question

Is there a Unity Pro system word that will provide the Quantum PLC Copro firmware version?

Issue:
   Quantum PLC copro version information

Product Line:
    Quantum
    Unity Pro

Resolution:
   %SW150 gives the Quantum Corpo firmware version.  It is displayed as a hexadecimal number.
Was this helpful?
What can we do to improve the information ?