Technical FAQs

Ask a Question

What is the memory capacity of the M580 processor ?

The M580 processor range offers the choice between 4 memory levels:
bb 4 MB for BMEP581020 processors
bb 8 MB for BMEP5820●● processors
bb 12 MB for BMEP5830●● processors
bb 16 MB for BMEP5840●● processors
Was this helpful?
What can we do to improve the information ?