Browse FAQs

What is the output current for the TM3DQ32TK?

Published date: 16 August 2019

Issue:
What is the rated output current for the TM3DQ32TK module?

Product line:
TM3, M221, M241, M251

Cause:
Questions with excessive current on the TM3DQ3TK relay output module.

Resolution:
The rated output current for the TM3DQ32TK is 100ma per point and max 2 amps per group.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.