Technical FAQs

Ask a Question

What is the part number for the M221 SD card?

Issue:
SD card part number for a M221 controller.

Product line:
TM221 PLC

Cause:
Unable to locate part number for the M221 SD card.

Resolution:
The part number for the M221 SD card is TMASD1. This is the only size available for use with the M221.
Was this helpful?
What can we do to improve the information ?