Browse FAQs

What is the maximum number of 140NOC78000 modules in a Unity project?

Published date: 30 November 2018

 

Title
140NOC78000 Module
 
Issue
Explain the maximum number of 140NOC78000 supported in a Unity project.
 
Product Line
Modicon Quantum.
 
Environment
Unity Programming software version 7.0 or greater
140NOC78000 firmware version 1.61 or higher
 
Resolution
A maximum of four NOC78000 modules are supported in a Unity project.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.