Technical FAQs

Ask a Question

What is the maximum number of connections supported on the BMENOC03x1 module?

Issue
Need to specify the maximum number of IO Scanner connections supported on BMENOC03x1 module configured through the Unity DTM browser.
 
Product Line
Modicon M580
BMENOC0301
BMENOC0311

Environment
ODVA Ethernet/IP 
Unity DTM Browser
 
Cause
N/A.
 
Resolution
The M580 Ethernet modules BMENOC03x1 supports a  maximum of 128 devices or Implicit client connections (Shared by EtherNet/IP and Modbus TCP) setup/configured through the DTM Browser

Was this helpful?
What can we do to improve the information ?