Technical FAQs

Ask a Question

What Telefast cables are needed for the TM221ME32TK?

The controller TM221ME32TK will need the following for the inputs

ABFT20Exxx and the ABE7E16EPN20 for the prewired

The outputs on the controller will both need the following

ABFT20Exxx and the ABE7E16SPN20
Was this helpful?
What can we do to improve the information ?