Technical FAQs

Ask a Question

What is the maximum number of 140NOC78000 modules allowed in rack?

Title
Maximum number of 140NOC78000
 
Issue
Maximum number of 140NOC78000 allowed in Quantum PLC System
 
Product Line
140NOC78000
 
Environment
Unity Pro
 
Resolution
 Even though the Quantum CPU can support a maximum of 6 Network option modules, it can only have a maximum of four 140NOC78000 modules.
From User Manual page 18,  A maximum of 6 communication modules can be configured on the local rack. Therefore, you can configure only four 140 NOC 780 00 modules. (For the remaining 2 communication modules, you can install a 140 NO• 771 •• or 140 NOM 2•2 00 module.) If you configure a 140NOC78 100 control head module on the local rack to manage a control network, you can only configure four 140NOC78000 modules on the local rack.
Was this helpful?
What can we do to improve the information ?