Technical FAQs

Ask a Question

Can the M340 BMXDDI1602 24VDC input module supprt NPN sensors?

Issue:
     Does the BMXDDI1602 IO module support NPN sensors or only PNP sensors?

Product Line:
     M340

Environment:
     Unity Pro

Cause:
     N/A

Resolution:
    No, the BMXDDI1602 input module is a sink (positive logic input).  As such, it does not support NPN sensors.
It supports PNP sensors.
 

Was this helpful?
What can we do to improve the information ?