Technical FAQs

Ask a Question

What are the restrictions of an unauthorized or unregistered copy of Proworx 32 or Proworx NXT software?

Title
What are the restrictions of an unauthorized or unregistered copy of Proworx 32 or Proworx NXT software?

Issue
There is no trial or demo version available for Proworx 32 or Proworx NXT software.

Product Line
Proworx 32 & Proworx NXT software

Environment
N/A

Cause
N/A

Resolution
An unauthorized or unregistered copy of Proworx 32 or Proworx NXT software will have full functionality.  The one restriction is that only 25 networks may be viewed and/or created.
Was this helpful?
What can we do to improve the information ?