Technical FAQs

Ask a Question

Is the TSX QUANTUM ETHERNET 10/100 BASE T100FX with Reference 140NOE77100 still commercialized?

The Reference 140NOE77100 is no longer commercialized, however could be replaced with 140NOE77101.
 
Datasheets:
 
140NOE77100, Ethernet network TCP/IP module - class B20 - data editor, rack viewer
https://www.schneider-electric.us/en/product/140NOE77100/ethernet-network-tcp-ip-module---class-b20---data-editor%2C-rack-viewer
 
140NOE77101, Ethernet network TCP/IP module - class B30 - data editor, rack viewer
https://www.schneider-electric.com/en/product/140NOE77101/ethernet-network-tcp-ip-module---class-b30---data-editor%2C-rack-viewer
Was this helpful?
What can we do to improve the information ?