Technical FAQs

Ask a Question

Proworx error: "323 - device not listening" followed by "328- driver turned off".

Issue:

Unable to connect to PLC.  Error is displayed.
Problem with the Modbus Plus timeout or connection.

Resolution:

 1/    Go to the Communications Setup and increase the Modbus Plus timeout.
  2/   Troubleshoot the Modbus Plus network.
Was this helpful?
What can we do to improve the information ?