Technical FAQs

Ask a Question

What causes 'Error #13 - wrong password' error when launching Proworx 32?

This can be caused if ProWORX 32 is being run on an unsupported Microsoft Operating System.
Delete the pwauthor.dat file and relaunch.
Was this helpful?
What can we do to improve the information ?