Browse FAQs

Does Unity Pro programming software run on Windows Server 2012?

Published date: 28 December 2018

Product Line
Unity Pro
 
Environment
Windows Server 2012 

Resolution
   Unity Pro v10 is qualified to run on Windows Server 2012.
It is not qualified to run on Windows Server 2012 R2.
Support for Windows Server 2012 R2 is to be added to Unity Pro version 11.1
 
 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.