Technical FAQs

Ask a Question

Why am I getting the error: "VJDTools... An invalid argument was encountered" when I create a Vijeo Designer application within Somachine? But I am able to open the Vijeo Designer project standalone.

This is caused by Windows UAC (User Access Control), which is limiting Vijeo Designer from launching within Somachine.  To resolve this issue you can turn off the UAC for that particular user, or run Somachine as an Administrator.

 
Was this helpful?
What can we do to improve the information ?