Technical FAQs

Ask a Question

Can execution order be turned off in Concept LD sections?

Yes, an edit to the Concept.ini file is necessary.  This file is found in the c:\windows folder.
The execution order is indicated by a number contained within parentheses next to the variable.

Go the LD section and add the following:

[LD]

;   Shows execution order (1 = show order; 0 = do not show order.)
ShowExecOrder=0


Concept should be closed when making changes to the concept.ini file.
This entry was added to  Concept in version 2.6 SR5.

 

Was this helpful?
What can we do to improve the information ?