Technical FAQs

Ask a Question

Can the M251 be setup as CANopen Master and Ethernet/IP slave?

The M251 model TM251MESC can be setup as a CANopen master and Ethernet/IP slave.  It handles up to 40 words in and 40 words out of data on the EIP slave.
Was this helpful?
What can we do to improve the information ?