Technical FAQs

Ask a Question

How to setup the USB RNDIS driver for the Unity Momentum PLC?

 

Title
Unity Momentum USB Communications capability
 
Issue
Need explaination of the USB communications setup of the Unity Momentum PLC.
 
Product Line
Modicon  Momentum
Environment
Unity
 
Cause
User inquiry.
 
Resolution
The Unity Momentum USB RNDIS driver uses a Ethernet type connection, this requires assigning the IP address of  90.0.0.2 to the Ethernet connection created by the installation of the Unity Momentum USB drivers in the computer Network Connections .
Was this helpful?
What can we do to improve the information ?