Technical FAQs

Ask a Question

Can the BMXNOC0402 module work on a BMX type backplane?

Title
BMXNOC0402 installation requirement

Issue
Need to specify the required backplane for the BMXNOC0401 module.
 
Product Line
Modicon M580

Environment
ODVA Ethernet/IP 
Unity DTM Browser
 
Cause
N/A.
 
Resolution
The BMXNOC0401 requires the use of the BME type backplanes in order to install the module into the PLC backplane.
They  can not be connected to the BMX type backplane.

Was this helpful?
What can we do to improve the information ?