Technical FAQs

Ask a Question

Is there a System Technical guide for the BMXNOR0200H module?

Title
BMXNOR0200H installation document

Issue
Need to explain the setup of a BMXNOR0200H module.
 
Product Line
Modicon 340

Environment
DNP3
Unity 
 
Cause
N/A.
 
Resolution
Yes, Attached below is the System Technical document for the BMXNOR0200H module.

Was this helpful?
What can we do to improve the information ?