Browse FAQs

What is the enclosure rating for the ATV61 Flange kits?

Published date: 13 March 2019

Issue
Customer wants to flange mount the drive, but is not sure if the Flange kit will maintain the enclosure rating. 


Product Line
ATV61, Altivar 61, ATV71, Altivar 71

Environment:
All models

Cause
Customer is flange mounting the heatsink. 

Resolution:
The flange kits are listed as IP54. 

IP5_ is dust-tight
IP_4 is protection against splashing of water

The equivalent NEMA rating would be NEMA 3 (NOT 3R). 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.