Technical FAQs

Ask a Question

When running redundant 140CPS124 00 power supplies, is it possible to replace a failed 140CPS124 00 with the 140CPS124 20?

No. Each power supply making up the redundant pair has to be of the same type. Mixing power supply models may result in unintended operation.

Was this helpful?
What can we do to improve the information ?