Browse FAQs

What is the meaning of the red 'R" on the icon for the M580 in the DTM browser ?

Published date: 29 November 2018

 

Title
M580 icon in the DTM browser
 
Issue
Need explaination of the red 'R' on the icon for the M580 CPU in the Unity DTM Browser.
 
Product Line
Modicon M580
 
Environment
Unity 8.0
 
Resolution
The M580 CPU icon in the DTM Browser has a red capital 'R' letter on its icon. The red 'R' on the icon in the DTM Browser indicates that the M580 embedded port is compliant with the "Device Ready" integration. Meaning that it will provide a higher level of integration for Scanners and Gateways into the M580 Ethernet architecture. For the initial M580 Unity 8.0 version support has been added for the PRM and Hart modules.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.