Browse FAQs

How is the BMXNOC0401 module setup?

Published date: 29 April 2019

Title
BMXNOC0401 intallation and setup

Issue
Need procedure to configure the BMXNOC0401 module.
 
Product Line
Modicon M340 

Environment
ODVA Ethernet/IP 
Unity DTM Browser
 
Cause
User configurable capability.
 
Resolution
The BMXNOC0401 is added to the Unity project by IO mapping the module into the PLC backplane. A Device DDT is created for the BMXNOC0401 that has Health bits and Control bits for monitoring and controlling the implicit connections that are setup for the BMXNOC0401 via the DTM Browser.
Once the module is added then to access the  configuration parameters:

  1. Double-click the BMXNOC0401 master communication DTM in the Unity Pro DTM Browser.
  2. In the navigation tree on the left side of the Device Editor window expand the Channel Properties

Use the Channel Properties page to:

  1. Select the Source Computer IP address to use for diagnosing or connecting to module or device DTMs to physical devices, and sending explicit messages to Modbus TCP and EtherNet/IP devices.

Use the Channel Properties - TCP/IP page to:

  1. Select a Configuration mode, which specifies how the BMXNOC0401 communication module obtains its IP addressing settings, and
  2. Edit the IP addressing settings that will be used if the Configuration mode is set to Static
  3. Do not enter a Gateway address unles an actual Gateway or Router is available on the connected network that can reply during BMXNOC0401 initialization.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.