Technical FAQs

Ask a Question

How is the EIP Slave Adapter capability of a BMXNOC0401 module setup?

Title
BMXNOC0401 EIP Slave Adapter capability

Issue
Need procedure to configure the EIP Slave Adapter capability of a BMXNOC0401 module.
 
Product Line
Modicon M340 

Environment
ODVA Ethernet/IP 
 
Cause
User configurable capability.
 
Resolution
The BMXNOC0401 supports up to 3 instances of local slaves (Local Slave 1, Local Slave 2, and Local Slave 3).

To Access settings:

  1. Double-click the BMXNOC0401 master communication DTM in the Unity Pro DTM Browser.
  2. In the navigation tree on the left side of the Device Editor window expand the EtherNet/IP Local Slaves.
  3. Select one of the three available local slaves.
To Configure parameters:
  1. Enable and name the local slave.
  2. Specify the size of the local slave input and output assemblies.
Was this helpful?
What can we do to improve the information ?