Browse FAQs

How is the EIP Slave Adapter capability of a M580 CPU setup?

Published date: 29 November 2018

 

Title
M580 CPU EIP Slave Adapter capability
 
Issue
Need procedure to configure the EIP Slave Adapter capability of a M580 CPU.
 
Product Line
Modicon Quantum
 
Environment
ODVA Ethernet/IP 
 
Cause
User configurable capability.
 
Resolution
The M580 CPU supports up to 3 instances of local slaves (Local Slave 1, Local Slave 2, and Local Slave 3).

To Access settings:
  1. Double-click the M580 CPU master communication DTM in the Unity Pro DTM Browser.
  2. In the navigation tree on the left side of the Device Editor window expand the EtherNet/IP Local Slaves.
  3. Select one of the three available local slaves.
To Configure parameters:
  1. Enable and name the local slave.
  2. Specify the size of the local slave input and output assemblies.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.