Technical FAQs

Ask a Question

Can the scan rate in a group be changed in Vijeo Designer?

Yes. From the Target Equipment, there are Scan Groups and they are as follows (Medium is the default).
Fast 50 - 250 msec
Medium 250 - 1000 msec
Slow 1000 msec
User Defined 2 sec to 60 min


Was this helpful?
What can we do to improve the information ?